I'm trying to write an AEL script and being overwhelmed. I am trying to run a series of simulations with swept variables and appending the values to a text file when the certain criteria are met. I've had intermittent success with
+de_analyze()+
and
+de_release_simulator()+
but cannot get them to function reliably.
Looking at this post:
run de_analyze() back to back
I though waiting until +desim_foreground_simulation_running()+ returned +FALSE+ could prevent a second simulation from starting. However, even long after the simulation finishes it returns +TRUE+. The only way I can stop the simulation is manually clicking the +Stop and Release Simulator+ command from the schematic window. Recoding this macro and adding it to the AEL script did not help either.
Here is simple snippet where it would get stuck for eternity.
-----
de_analyze();
while(desim_foreground_simulation_running())
{
sleep(1);
fputs(stderr,sprintf("desim_foreground_simulation_running: %d", desim_foreground_simulation_running()));
}
-----
Is there a concrete way to determine if a simulator is running, and how to release it?