AnsweredAssumed Answered

External Sequence InterfaceParms Output TestExec 6.1

Question asked by rene.campos@continental-corporation.com on Nov 20, 2015
Latest reply on Dec 3, 2015 by Ever
Hi, 

I have a couple of testers with TxSL 6.1.2. In this version of TxSL when calling a Sequence and expecting a return value from the InterfaceParms, if the Parameter is set as Output, the value of this parm will be set to +Null+ if its a String  type or 0 if it is Real or integer.

Is there a patch for this issue? I know this feature works correctly in TxSL7.1. 


Thanks, 
Rene  

Outcomes