AnsweredAssumed Answered

Using the Equation Based function

Question asked by VegardMi on Feb 21, 2016
Latest reply on Feb 22, 2016 by BarrettP

Hello.

I was wondering if anyone knew if it is possible to use variables from "Parameters" in the Equation Based function in EMPro? 

Using parameters to set up the max and min values for "u" and "v" works fine, but I am not able to use parameters in the "x", "y" and "z" sections. 

I want to use this function to make a parameterized Vivaldi antenna.



Vegard

 

Edited by: VegardMi on Feb 22, 2016 12:40 AM

Outcomes