AnsweredAssumed Answered

Converting MATLAB-based Complex Vector into Waveform File

Question asked by matlabuser on Jul 13, 2015
Hi all,

I want to take vectors/arrays created in MATLAB and generate waveform files which can be transferred, using a USB memory stick, onto an 81180A AWG or an E8267D VSG.
I do not have physical access to the AWG/VSG so I cannot use the iqtools application.

I came across the 'convert to arb' function (http://www.mathworks.com/matlabcentral/fileexchange/34840-convert-vector-to-arbitrary-waveform) but it says it is applicable for the 3352xA generator.
Does anyone know if it can be used for the AWG/VSG I mentioned above? If not, is there any other readily available function to convert to the 81180A andn E8267D?

Thanks in advance,

Jimmy  

Outcomes