AnsweredAssumed Answered

ECal kit presence and characterisation info on E5071C

Question asked by nar_bra on Dec 15, 2015
Hi,
I want to be able to detect presence of ECal kit when this is connected to e5071C and to receive information like in pop up windows on e5071C (Characterization Info). However, seems to be that directly SCPI commands are not available ?
Command: SENS1:CORR:COL:ECAL:UCH CHAR0(CHAR1)  only select Factory or User1. How can I get information about ECAL, like Cal. data, ID etc. ?
Secondly, if is possible to read information from ECal itself if this is not connected to network Analyzer ?

Best regards,
nar_bra  

Outcomes