AnsweredAssumed Answered

AEL Error Catching

Question asked by slepkow on Jan 26, 2016
Hello All,

I'm trying to write an AEL function to catch errors during simulation. Essentially, this error is caused when an SDD block equates to a zero resistance and causes a convergence error. If this error occurs I'd like to adjust a parameter in the design and re-simulate.

I tried the +on_error+ function but it does not seem to be triggering.

Additionally, how can I wait for a simulation to complete before progressing in the code? Along the lines of

+while(Simulator Running OR NOT Timed Out) {Do Nothing}+

Thanks  

Outcomes