AnsweredAssumed Answered

33500B to BenchVue

Question asked by rickwhatson-triot&m on Sep 13, 2015
Latest reply on Sep 14, 2015 by rickwhatson-triot&m
I have tried connecting a 33500B to BenchVue.

Everything seemed to work correctly using the USB cable, but if I try to connect using Ethernet I get the following error:

The instrument initially appears to be available to make a connection.
If I double click on it or drag it into the workspace, it starts trying to make the connection.
After a while it gives this message:  "VISA connection with instrument has been lost."

Are there some settings I need to change, or drivers I need to update to solve this?

I am using BenchVue Version 2.7.1505.22 and the checker says this is up to date.
Running on Windows 8.1 64bit
Ethernet cable connection 33500B to router, WiFi connection to PC.

Thank you

Edited by: Rick Whatson - TRIO T&M on Sep 13, 2015 10:55 PM  

Outcomes