AnsweredAssumed Answered

PNA MArker Question

Question asked by Ballschmieder on Dec 7, 2011
Latest reply on Dec 7, 2011 by daras
Hello,
I have a N5230A with which I need to make a flatness measurement with. The span of the S21 measurement is from 5.5 - 11.5 GHz. The specification for the measurement is +/- 1dB over any contiguous 500MHz BW of the 5.5 - 11.5 GHz span.

My thought for making the measurement was to use 2-markers, 500 MHz apart and measure their amplitude difference as they are moved together across the measurement span.

Can this be done with the N5230A?

Thank you, Ken  

Outcomes