Hi,
A saved *.bin waveform can be loaded back into the oscilloscope.
Question: Is it possible to adjust the loaded waveform such as scaling?
Owen
A saved *.bin waveform can be loaded back into the oscilloscope.
Question: Is it possible to adjust the loaded waveform such as scaling?
Owen
The answer somewhat depends on knowing this.
On Infiniium scopes, in general, stored data (including .bin) is loaded into a memory waveform. Depending on the SW version, you can do things like right-click on the waveform to get access to the scaling controls, or use a pull-down menu for the same things. On some versions you can attach, for instance, the m1 waveform to the Channel 1 controls so turning the vertical knobs will do vertical scaling. You can also tie the memory waveforms to the scope horizontal controls, so turning the horizontal knob will change the time scale.
Al
Disclaimer: For more reliable response, you should consider calling your local Keysight Technical Call Center. The Keysight Forums are monitored on an "as available" basis, and aren't necessarily the fastest way to get technical questions answered.