what is the difference between W3631A and W3636A (non-stacked) DDR3 x16 command and data probes ?
what does it mean, non-stacked ?
My DUT is running with a single chip of MT41J128M16 (16 Meg x 16 x 8 Banks), DDR3-1600.
which one of mentioned above is correct to order ?
what does it mean, non-stacked ?
My DUT is running with a single chip of MT41J128M16 (16 Meg x 16 x 8 Banks), DDR3-1600.
which one of mentioned above is correct to order ?
As stated in various places throughout the forums, they are intended for peer-to-peer interaction, and they are not a replacement for contacting the Technical Call Center at Keysight directly. They are not monitored on a regular basis by any Keysight personnel.
If you want a quick, reliable answer about product-related issues in the future, please get in touch with the Technical Call Center.
Al
When looking at the Micron data sheet for the MT41J128M16 (page 17 pinout image) the chip doesn't appear to have multiple chip selects however when searching for information on the part you're using there are multiple parts that begin with this number that also have a suffix (-xxx). Please check for the exact information on your part.
The W3630A series data sheet also lists what signals are NOT available for a given BGA interposer (see page 7 of the following: http://literature.cdn.keysight.com/litweb/pdf/5990-3179EN.pdf?id=1648244). You would use the W3631A if you don't need access to A15 or BA2.