AnsweredAssumed Answered

Trigger output polarity on 8164B

Question asked by brian_henderson on Jul 24, 2015
Latest reply on Jul 28, 2015 by mkelly
Is it possible to change the trigger output polarity to falling edge instead of rising edge on the 8164B? I am sweeping an 81600B tunable laser and I would like to output falling edge triggers during the sweep instead of rising edge. 

Page #69 of the 8164B manual seems to indicate that the default mode is rising edge.

"The trigger level at the external trigger connectors is by default active high..."

I am hoping that means that I can change it to falling edge but I haven't found a command or setting to configure the polarity.

Thank you,
Brian  

Outcomes