B4621A DDR bus decoder installation provides some default configurations for 16962A board
and BGA interposers.
Is it available a default config for DDR3, x16 32bit (similar to DDR2, x16 32bit, which is available) ???
Which BGA interposers have to be used for 32bit and how many 16962A boards (2 or 3) ??
DDR3 - 1600.
I found, there is only 16962A, DDR3 x16 16bit default config is included to B4621A setup.
Thank you!
and BGA interposers.
Is it available a default config for DDR3, x16 32bit (similar to DDR2, x16 32bit, which is available) ???
Which BGA interposers have to be used for 32bit and how many 16962A boards (2 or 3) ??
DDR3 - 1600.
I found, there is only 16962A, DDR3 x16 16bit default config is included to B4621A setup.
Thank you!
Did you use the DDR Setup Assistant?
If you use that, and answer the questions correctly, it should find the correct configuration file.
If you don't have that available, then you haven't loaded all of the necessary tools?
Al
Disclaimer: For more reliable response times, you should consider calling your local Keysight Technical Call Center. The Keysight Forums are monitored on an "as available" basis, and aren't necessarily the fastest way to get technical questions answered.