AnsweredAssumed Answered

What is the difference in oscilloscope 5032 vs. 3032 with single-triggering

Question asked by Ever on Aug 24, 2015
Latest reply on Aug 24, 2015 by Ever
Hello,
we are using the oscilloscope 5032 and have some working programs that send SCPI-commands.
Now we switched to the 3032 oscilloscope which behaves different at triggering.
Here are the commands that used to work:

*RST
:CHAN1:SCAL 5V;OFFS -4;COUP DC;IMP ONEMeg;DISP 1;BWL 1;INV 0;UNIT VOLT;PROB 1;
:TIM:MODE MAIN;SCALE 0.01;REF LEFT;POS 0;
:STOP
:TRIGger:SWEep AUTO
:SINGLE

The problem is:
-> The 5032-scope executes a new sweep after i send the SINGLE-command. 
-> The new 3032 does..... nothing.....
Do i have to use the "new" ForceTrigger?

Also when i manually press the single-button at the 5032 instrument the sweep is starting. 
And it does not sweep on the 3032???

Is there something new at 3032 that is missing?

Thanks
BR
TM  

Outcomes