AnsweredAssumed Answered

'Implement' LRM calibration

Question asked by labdevo on Jul 27, 2015
Hi,

I want to perform an LRM calibration and I already have the Standards.
However, I have no idea how to implement this Calibration-procedure in the PNA-L N5230A.
In the Calibration-Wizard, I can choose 'Unguided-Calibration' which opens the dialog box 'Select Calibration Type for mechanical Standards'. In this dialog box I can choose for example '2 port calibration' or TRL, but there is no possible selection for LRM. 
So how it is possible to 'implement' LRM into the VNA? Or can I choose also TRL for LRM because of the same algorithm?
I hope someone could help me :)

Best regards  

Outcomes