AnsweredAssumed Answered

Frequency Blanking, Instrument State, and Cal Sets, oh yeah....

Question asked by andeezlemoyo on May 29, 2015
Hi,

I am working with an 2-port E8362C, running firmware version, A.09.42.22. Using DCOM.

From the PNA Docs, A09.09,  Under the document, "Frequency Blanking," heading, "Instrument State and Cal Sets," bullet #3.

"When later applied to a channel, if the Cal Set has a higher security level than the current system security level, the system security level will become upgraded to that of the Cal Set."

Uh uh.  Not what I'm observing, which is a problem.  Can someone please verify?

Thank you,

Andy  

Outcomes