I wish to congratulate the software developers team of Keysight Handheld Meter Logger Software, finally after four years time they did implement an High/Low limits audible alarm function.
But there is something more needed as improvement, they should add an option so the user to choose his own preferred wave file as audible alarm.
Additionally I can not understand why this is so impossible, an user to send feedback to specific software developers by direct communication?
Just add an option in this 450 megabytes of software with the tittle : Send us your feedback.
But there is something more needed as improvement, they should add an option so the user to choose his own preferred wave file as audible alarm.
Additionally I can not understand why this is so impossible, an user to send feedback to specific software developers by direct communication?
Just add an option in this 450 megabytes of software with the tittle : Send us your feedback.
1) The installer does not offer an option so a User who does not own any special Licenses, him to avoid installing needles software to his computer.
As for example: Keysight Licence manager, Keysight Licence agent, Agilent host processor platform (what ever this is).
2) The installer does not create any program icon at windows desktop or at windows programs menu at windows XP Pro SP3, about the most important than all software = this Handheld Meter Logger.
3) The addition in this software about making it own reports for printing, this causes an error condition at least in my computer that I am using Microsoft Office small business 2003, and I am getting an error screen mentioning :
4) System.Runtime.InteropServices.COMException (0x800A140C): Word cannot start the converter mswrd632.wpc
5) In this last problem responsible software this could possibly be NET framework 4.6 commands, which them are supported by newer windows version, because Microsoft decided that windows XP users them will never receive a higher version than NET framework 4.0
6) By using MicrosoftFixit50352.msi this trying to unregister mswrd632.wpc but other problems shown up, and for them responsible is the engine of Handheld Meter Logger.
I do wish or hope Keysight software developers them succeeds making the forms creation to work properly, mostly because this is an equivalent to FLUKE forms software which this is something that Keysight does not have in their offerings and this is useful for professional electricians.