AnsweredAssumed Answered

Checking calkit standard model parameters in firmware for an E5061B

Question asked by b.hall on Jun 30, 2015
Latest reply on Jul 17, 2015 by drkirkby
What is the best way for a user to inspect the calkit standard definitions in firmware on an E5061B? 

One option may be to proceed as if to modify values (as described here) and then just look at the current firmware value, but that seems risky (one might inadvertently change values). So I wondered if there is an alternative.

Also, I notice that the standard model values are no longer available for many VNAs (here) . The entries often simple refer to firmware definitions. The manual accompanying the calkits also seem now to refer to this web URL, whereas in the past values were included. This was not the case a few years ago. Why has it changed?  

Outcomes