Hi Milan. Keysight uses the "CFGxxx" designations to show what options were installed at the factory. In the case of a 33522B-CFG011, the unit was configured at the factory as a "Waveform Generator, 30 MHz, 2 channel, with arb with option 000,SEC,MEM,IQP. In other words, it was configured and shipped as a 2-channel 30 MHz waveform generator with upgraded memory, the NISPOM Security option, and the IQ player upgrades installed.
Edited by: gemsupport on Jun 23, 2015 2:15 PM