AnsweredAssumed Answered

DSO3102A cant save in USB

Question asked by theamberco on Jul 16, 2015
Latest reply on Aug 6, 2015 by ksmith
I have the above oscillsocope and it has the lastest firmware and it also have the N2865A USB module.
Everything Works fine and module and USB stcik are detected but when I try to save to the USB after I press save nothing happens and sometimes I get File Utility Error message. I have another oscillsocope the same with another USB module the same and I got the same thing. I used two different USBs 2 and 4 Gb and formated them NTFS and FAT but the same problem I cant save into the USB stick. Any ideas why this happend.  

Outcomes