I want to do the em-cosimulation of a power amplifier circuit board, and the substrate is CPWG.
Please see the attached picture(layout.png), and that's the output matching of the power amplifier circuit.
I have set 7 port.
Port1(P1),Port2(P2),Port3(P3) for input, output,DC bias
Port4(P4+,P5-),Port5(P6+,P7-),Port6(P8+,P9-),Port7(P10+,P11-) for placing SMD components.
My substrate is as (substrate.png),
For the CPWG substrate, I have few questions:
1. For the cond, I don't know what is the difference between "sheet" and "Intrude into substrate" ?
2. Is it right to place via at substrate to let the metal beside the signal metal be grounded?
For the port calibration,
I've set "TML" for the input,output,and dc port, and set "SMD" for the ports which are for placing the SMD component.
I set the em simulation frequency from 0~2GHz, but when the simulation start, there are some warnings:
"Layout healing changed the layout. The actual
highest aggregate snap distance was 0.04 mm.
Further details have been written to the DRC
report."
"The port setup needed to be corrected:
Calibration will not be used for port "P6" (pins
"P4" and "P5" are not on the edge between a
conductive and a nonconductive region)."
And all the SMD ports have the same message.
I change the calibration "SMD" to "None", and there is only the first warning left.
The result is as (result.png)
I don't know why can't I choose SMD calibration??
Besides,the result only shows S11,but I have more than one port!?
My final goal is to simulate the schematic and see the Zin at 2GHz.(final.png)
But it has an error:
"Error detected by hpeesofsim during netlist parsing.
`(' illegal: valid characters in design names are alphanumeric or _`@#&+-=^
define "Output_Match_layout(2)" ( P1 P2 P3 P4 P5 P6 P7 P8 P9 P10 P11 Ref=0 ))
But I didn't change the Pin name.
Does anyone have idea??
Thanks for replying~~
ps. I've attached my workspace.(Outputmatching_wrk.7z)
Edited by: jeff0283 on Jul 16, 2015 9:38 AM
Please see the attached picture(layout.png), and that's the output matching of the power amplifier circuit.
I have set 7 port.
Port1(P1),Port2(P2),Port3(P3) for input, output,DC bias
Port4(P4+,P5-),Port5(P6+,P7-),Port6(P8+,P9-),Port7(P10+,P11-) for placing SMD components.
My substrate is as (substrate.png),
For the CPWG substrate, I have few questions:
1. For the cond, I don't know what is the difference between "sheet" and "Intrude into substrate" ?
2. Is it right to place via at substrate to let the metal beside the signal metal be grounded?
For the port calibration,
I've set "TML" for the input,output,and dc port, and set "SMD" for the ports which are for placing the SMD component.
I set the em simulation frequency from 0~2GHz, but when the simulation start, there are some warnings:
"Layout healing changed the layout. The actual
highest aggregate snap distance was 0.04 mm.
Further details have been written to the DRC
report."
"The port setup needed to be corrected:
Calibration will not be used for port "P6" (pins
"P4" and "P5" are not on the edge between a
conductive and a nonconductive region)."
And all the SMD ports have the same message.
I change the calibration "SMD" to "None", and there is only the first warning left.
The result is as (result.png)
I don't know why can't I choose SMD calibration??
Besides,the result only shows S11,but I have more than one port!?
My final goal is to simulate the schematic and see the Zin at 2GHz.(final.png)
But it has an error:
"Error detected by hpeesofsim during netlist parsing.
`(' illegal: valid characters in design names are alphanumeric or _`@#&+-=^
define "Output_Match_layout(2)" ( P1 P2 P3 P4 P5 P6 P7 P8 P9 P10 P11 Ref=0 ))
But I didn't change the Pin name.
Does anyone have idea??
Thanks for replying~~
ps. I've attached my workspace.(Outputmatching_wrk.7z)
Edited by: jeff0283 on Jul 16, 2015 9:38 AM