AnsweredAssumed Answered

Adaptive pin location for optimization in Momentum

Question asked by Zeid on Jan 22, 2016
Latest reply on Jan 28, 2016 by volker_muehlhaus
Hi,

I am optimizing a parametric model in Momentum. Among the ports, some have a "None" calibration type and the corresponding pins are placed inside a metallic pad without being "snapped" to a specific interconnect.
For that case, when running the optimization, the pin's position is fixed relative to the origin but as the geometry is being optimized, the intended locations of such pins with regard to pads are lost. (It even can end up that a pin is not anymore in contact with the conductor).

How to fix/link such pins to a specific position inside the metallic pad so that they will be kind of attached to it as the geometry is being optimized?

Sincerely,
Zeid

Edited by: Zeid on Jan 22, 2016 9:41 AM

Edited by: Zeid on Jan 22, 2016 9:42 AM

Edited by: Zeid on Jan 25, 2016 12:56 AM  

Outcomes