AnsweredAssumed Answered

Can E8358A have CPU board upgrade?

Question asked by mirek on Jul 13, 2011
Latest reply on Jul 13, 2011 by odanzy
I wonder if the old two ports E8358A Network Analyzer can have CPU board upgrade. The unit that I have is with 266MHz cpu and 64MB RAM and Window 2000. I know that after 2002 this model had 500MHz cpu board.
Can this Network Analyzer be upgraded with 500Mhz or even 1.1GHz CPU board?  

Outcomes