If you mean saving screenshots, then there are several options:
_*Save to USB drive*_ - Plug in a USB thumbdrive. - Press the "Save|Recall" button. - Press the "Save" softkey. - In this menu, select the desired format to save (PNG, BMP8 or BMP24) and the destination. - Press "Press to Save".
_*From the web interface*_ If the scope is connected to LAN, you can access the web interface and click on the "Get Image" button on the left side of the webpage.
_*BenchVue*_ Screenshots can also be obtained from the BenchVue software.
_*Save to USB drive*_
- Plug in a USB thumbdrive.
- Press the "Save|Recall" button.
- Press the "Save" softkey.
- In this menu, select the desired format to save (PNG, BMP8 or BMP24) and the destination.
- Press "Press to Save".
_*From the web interface*_
If the scope is connected to LAN, you can access the web interface and click on the "Get Image" button on the left side of the webpage.
_*BenchVue*_
Screenshots can also be obtained from the BenchVue software.