AnsweredAssumed Answered

Delay of a circuit board trace.

Question asked by theamberco on Sep 6, 2015
Latest reply on Sep 13, 2015 by mikejvir-
Hi, I want to know the delay of a circuit board trace it would be very hard to measure the cross section to calculate the C or L. So can I use two microprobes (of known lengths) and put on microprobe pin on the trace and the other for example if I want to measure the Capacitance of a trace where would it go?. I have no time domain, so Is it possible to get the length and velocity factor without time domain in a VNA?
thanks.  

Outcomes