I want to do two layer metalization EM Simulation using ADS2011.10.
I am getting following difficulties while generating EM Simulation and layout generation of two layer metalization using ADS2011.10
1) I want to get the two layer metalization as shown in the screen shot of TWO_LAYER_LAYOUT_EXAMPLE. I am not getting as shown in the screen shot of TWO_LAYER_LAYOUT_EXAMPLE. When I opened and viewed 3D, Obtained 3D view as shown in the screen shot of 3D_View_Two_Layer_Metalization. How to get the two layer metalization 3D as shown in the screen shot of TWO_LAYER_LAYOUT_EXAMPLE.
2) In the substrate view, can we get the two layer metalization as shown in the screen shot of TWO_LAYER_LAYOUT_EXAMPLE. If so, how we can get, what modification can be done to obtain.
3) I generated the EM Simulation using ADS2011.10 for two layer metalization. I have attached the .Zap file of two layer metalization, which is shown in EM_Simulation_2_wrk.7zap. Whatever I have done for the two metalization EM simulation, is it correct. If it is wrong, what mistake I have done, can you show me.
Can you clarify above difficulties
I am getting following difficulties while generating EM Simulation and layout generation of two layer metalization using ADS2011.10
1) I want to get the two layer metalization as shown in the screen shot of TWO_LAYER_LAYOUT_EXAMPLE. I am not getting as shown in the screen shot of TWO_LAYER_LAYOUT_EXAMPLE. When I opened and viewed 3D, Obtained 3D view as shown in the screen shot of 3D_View_Two_Layer_Metalization. How to get the two layer metalization 3D as shown in the screen shot of TWO_LAYER_LAYOUT_EXAMPLE.
2) In the substrate view, can we get the two layer metalization as shown in the screen shot of TWO_LAYER_LAYOUT_EXAMPLE. If so, how we can get, what modification can be done to obtain.
3) I generated the EM Simulation using ADS2011.10 for two layer metalization. I have attached the .Zap file of two layer metalization, which is shown in EM_Simulation_2_wrk.7zap. Whatever I have done for the two metalization EM simulation, is it correct. If it is wrong, what mistake I have done, can you show me.
Can you clarify above difficulties
Attachments
> You have the bottom of the board in the substrate definition set as Cover, that gives a continuous metal layer. To see double side board configuration you need to set that instead as a strip plane and map the cond2 metalization to that side of the board.
Where I have to go and change the options to get the double side configuration. Can you suggest me.
What about other points difficulties in the posting #1.
Attachments
So in the substrate editor select the lower interface and set the "Bounding area layer" back to none.
Then for this lower interface right click and set "Map Condictor Layer" and configure cond2 with all the required material and thickness properties.
Save and exit the substrate editor and it should work.
Here with I am attaching EM simulation of two layer metalization ".zap" file. I have EM simulated using ADS2011.10 for two layer metalization. I am new to this ADS2011.10 for two layer metalization EM simulation.
I have already done the EM Simulation for two layer metalization. I request you to check once the ".Zap" of two layer EM simulation and tell whether it is correct for all settings of EM Simulation of two layer metalization. If there is any mistake, can you point out me.
Can you help me.
Attachments
FYI - you do not need two subsstrate definitions, substrate1 and substrate2. Only substrate1 is required and that is the only one used.
> GND pins on EM port not correctly define ("No explicit pin is assigned to minus terminal while there are no infinite ground or slot layers defined in the substrate. This port setup can lead to inaccurate or unphysical results" according to balloon help message in ADS 2015.01).
Thanks for your valuable advices for better design, you have advised me lot many issues, which can be modified in my design. I change all the bad design choices.
How we have to make EM ports to correctly define, what changes can be made to get EM ports correctly. Can you suggest it.
Attachments