AnsweredAssumed Answered

PNA-X downgrading firmware from 10.4X back to 10.25 or lower versions

Question asked by rok on Sep 9, 2015
Latest reply on Sep 25, 2015 by Dr_joel
Hi,

Was just wondering if there will be any issues downgrading the firmware from a 10.4X (i.e. 10.40 or 10.43) back down to a lower version. (like 10.25) The reason for asking is that the 10.4X firmwares also changes something in the DSP area (necessitating several reboots), and so I'm not sure if it will have some side effects or not.

Just wondering,
rok  

Outcomes