AnsweredAssumed Answered

U2004A unsupported in BenchVue.

Question asked by ahiggins on Jan 11, 2016
Latest reply on Jan 11, 2016 by w0dz
I've confirmed that the U2004A is shown as connected with the Keysight Connection Expert, and I'm able so send commands to the instrument; however, when I open BenchVue, the device is listed with a green checkmark but is unsupported. Is there something I can do to communicate with the device in BenchVue?

It's connected directly to my computer (Windows XP SP3 - I can't change the OS) via USB.

Edit: I'm using BenchVue 2.7 and IO Library version 17.1.20011.4
Edited by: ahiggins on Jan 11, 2016 9:18 AM
Edited by: ahiggins on Jan 11, 2016 9:18 AM  

Outcomes