AnsweredAssumed Answered

sweep averaging vs. point averaging

Question asked by drkirkby on Jan 10, 2016
Latest reply on Jan 11, 2016 by drkirkby
Can anyone tell me the relative advantages/disadvantages of point vs sweep averaging? I assume that the two averaging methods used by the PNA are similar/identical to that in the attachment. Is that correct? This was taken from the manual of an HP 4291B impedance/material analyzer, but there's no mention of the benefits of either, and I don't see it mentioned in the PNA documentation either. 

Dave  

Attachments

Outcomes