AnsweredAssumed Answered

VIAs in the Layout created Component

Question asked by gigan on Aug 14, 2015
Simple two-layers strip structure with VIAs as example (See pictures)

Why there are no VIA in the Symbol of created in the ADS Layout and in the circuit using that symbol? 
How to make them (VIA) visible ?

Can some one explain/help?

Edited by: Gigan on Aug 14, 2015 1:21 AM

Edited by: Gigan on Aug 14, 2015 1:44 AM  

Attachments

Outcomes