AnsweredAssumed Answered

PNA-X strange csa loading behavior for A.10.45.03 firmware

Question asked by rok on Mar 4, 2016
Latest reply on Mar 10, 2016 by johanericsson
Hi,

I'm running the PNA-X with the A.10.45.03 firmware. I am having problems reloading the 'test2.csa' file which is attached. However, I don't have a problem reloading 'test1.csa' file. The 'test2.csa' is derived from 'test1.csa' by just modifying the RF input power values for the various channels and modifying the window titles. So I'm not sure why I can't reload the 'test2.csa' file which is the one I want to use. Additionally, I tried reloading the 'test2.csa' file on another PNA-X running a new A.10.49.03 firmware, but it doesn't work as well. If your team can analyze the 'test2.csa' file to see what's wrong, that would be greatly appreciated.

Thanks,
rok  

Attachments

Outcomes