AnsweredAssumed Answered

14585A funtionality by using SCPI commands

Question asked by Nacho on Nov 30, 2015
Latest reply on Jan 14, 2016 by MattC
Hi

N6705B / 6781A / 14585A / is a great combo! It is flexible to make current consumption logs.

Simple question, how-to make same measurement by using SCPI commands.
* Example device is 4.2V li-on powered handheld.
* Measurement duration variates from 5s to 10h
* After measurement same .dlg as in 14585A will can be found from PC.
Additionally
* min/max/avg can be found from PC in txt format
* picture of the graph/plot can be found from PC  

Outcomes