Agilent had not long ago posted a real list of compatible printers for the infiniivision scopes but it has since been replaced by the blanket statement at this URL:
[http://www.keysight.com/main/editorial.jspx?cc=US&lc=eng&ckey=1379987]
I have a MSO-X-3104A that does not have windows and is very fussy about printers. Not all PCL5 printers work. Many color printers will only print B&W. The list is now gone.
Can anyone supply the list for me?
Thanks,
Jason K
[http://www.keysight.com/main/editorial.jspx?cc=US&lc=eng&ckey=1379987]
I have a MSO-X-3104A that does not have windows and is very fussy about printers. Not all PCL5 printers work. Many color printers will only print B&W. The list is now gone.
Can anyone supply the list for me?
Thanks,
Jason K
Since:
1) The number of tested printers is much smaller than the number of available printers,
2) Printers get obsoleted, or go 'out of support' by the manufacturer, very quickly,
3) There are other means for getting printable information, such as screenshots out of the scope and onto the printed page,
4) The vast majority of tested PCL3 and PCL5 printers worked well, if not perfectly,
5) There's a considerable cost in time and money acquiring and testing each printer with each scope,
6) Those resources are limited, and would be better spent in developing new scopes, or adding new features to existing scopes,
a decision was made to stop testing printers, and provide the blanket statement that's now available on the web. It is not a perfect solution, and we apologize, but it seemed to make the most sense for most users and in most situations.
Al