AnsweredAssumed Answered

SPCI Command for Bandwidth String on 8720C

Question asked by anguilin on Apr 22, 2015
Latest reply on Apr 27, 2015 by RayH
Hello Fellow RF Community,
I have programmed (using .NET) a couple of applications which utilizes the command:

'CAL:MARK:BWID -3'

then it brings in a string which I can convert into an array and pick out the meausrements I want.

Although the 8720 has front panel buttons which give me me the -3dB information (e.g. Q, center freq, IL) I am unable to find this in the API. 

Can someone give me a hint as to what command I use to send to the VNA so I can read the bus and get this string?

http://na.support.keysight.com/pna/help/latest/Programming/XComFinderSet.htm  

Outcomes