Hi, I am designing the LNA for the band 0.5 - 4 GHz. I found some LNAs (like MGA61563, MGA72543,...) of Avago and tried to use the ADS model of these LNAs.
However, when I imported the LNAs' model with format *.deb file into ADS 2013 (according to the guideline), I can't found this model in the Component Library, though I can view them in the list of installed packages by using command : "hpeesofpkg --list" in Command Prompt.
It seems that this model is only used in the old version of ADS, and I must use the *.s2p file to simulate them?
If anyone can help on this it will be a great help.
However, when I imported the LNAs' model with format *.deb file into ADS 2013 (according to the guideline), I can't found this model in the Component Library, though I can view them in the list of installed packages by using command : "hpeesofpkg --list" in Command Prompt.
It seems that this model is only used in the old version of ADS, and I must use the *.s2p file to simulate them?
If anyone can help on this it will be a great help.
"We in Avago have not progressed above ADS 2012. You will need to roll back to ADS2012 or ADS2009 to use the ADS model for the MGA-61563.
I believe we may get the go ahead to update to ADS 2014 soon."
I still recommend that you contact them directly about this issue.