AnsweredAssumed Answered

N5230 Firmware

Question asked by jgraygoza on Feb 18, 2009
Latest reply on Feb 18, 2009 by odanzy
Hello,

If anyone can provide help on this,
I wil appreciate it very much.

Whenever I try to upgrade firmware on a PNA,
I am encountering the issue that right before is done removing the current version to install the new one,
a message pops up saying that it can not remove a COM+ application.
Now, I could ignore or cancel.

If I cancel, the version stays the same.
But I choose to ignore,
it will remove the version and when it tries to install the new one,
it will not be able to finish because a message at the very end will popup saying that it could not register COM+ application.
This happens because the previous one was not removed.
Can anyone help on this matter?
Is this just a matter of privileges?
Or is there anything else I can do to clean this up?

I have encountered this just about anywhere and can't seem to find a fix for it.
Any help would be greatly appreciated.

Thank you very much.  

Outcomes