AnsweredAssumed Answered

Trigger settings for DMM 34450A

Question asked by vgkarthik88 on Apr 9, 2015
Latest reply on Apr 24, 2015 by Tardz
Hi, I am trying to setup an experiment to measure the current of a device during processing. I would like to send a trigger from the device to the DMM to start the measurement at a given time. I am not able to find the correct settings to use for the trigger input i.e what voltage i should use for the trigger pulse, what is the minimum length of the pulse. 

also, would it be possible to stop the measurements once i am done with the processing? The length of time required for processing will vary so i cant just set a precalculated number of readings for the DMM.  

Outcomes