AnsweredAssumed Answered

Avago ATF-34143 model simulation error:frequency dependent

Question asked by jackey_wan on Dec 31, 2015
I used unarchive import by .Zap
and new a sch to using that

but I want to test the model can work
so the 4 pin all Gnd
I run the DC is OKay
but run S-parameter or transien Error:
This error typically caused by using a frequency dependent model of dielectric losses while setting Er=1.
Set DielectricLossModel to'FrequencyIndependent' or TanD=0
so I change the transmission line's K , it is normal work
I don't understand that model has something wrong or something problem with my step 
if the K from 1 to 1.1 will effect a lot?

Edited by: jackey_Wan on Jan 1, 2016 12:38 AM  

Attachments

Outcomes