AnsweredAssumed Answered

34970A in RS232 and 34972A in LAN together using datalogger not working

Question asked by dan_hfc on Mar 25, 2015
When I run 34970A alone using  RS232 it works correctly.  When I add 34972A in LAN mode data collection will not start.  Both instruments are found and are connected to without a problem.  Both are connected the same in the scan lists.  The 34972A LAN works fine when the 34970A is not present.
When I run two 34972A together they operate correctly.
The help file says that the software can run these two instruments together.  The 34790A is attached to com1. No other instruments are on the serial ports.

What is the problem?  

Outcomes