AnsweredAssumed Answered

Prevent update of the PNA firmware

Question asked by andeezlemoyo on Mar 10, 2015
Latest reply on Mar 13, 2015 by daras
Hi,

I am working with an 2-port E8362C, running firmware version, A.09.42.22. Using DCOM.

Is there a way to prevent the PNA software (firmware) from updating while I make changes to the instrument state, traces, windows, channels, etc.?  An example of what I would like would be when recalling a .csa file, using the PNA, with an extensive instrument state, the display just appears after it is loaded.  When I create instrument states using DCOM, each change is immediately reflected in the firmware. I would like to suspend the display while I make changes via DCOM. The resume the display when I am done. 

Thank you,

Andy  

Outcomes