AnsweredAssumed Answered

Changing the Microsoft.NET Framework Version ?

Question asked by paulrowan on Mar 24, 2015
Latest reply on Mar 25, 2015 by WDrago
I'm having problems with the serial event handler (eventDisposed works fine) but eventDataRecived does not execute but eats 50% CPU time and then locks VEE if I close the serial port. (all works fine in VS c#)

I have .NET framework v2 and v4 installed on my development machine and was wondering if using v4 might be the answer, the .Net Assembly References dialog picks up the location of the v2.
If I browse to the v4.0.30319 directory "System.dll" errors as not being an valid .NET assembly ?

Is there a way to get VEE to use the v4 framework ?

VEE 9.3.15 under Win7 Pro.  

Outcomes