AnsweredAssumed Answered

Marker readings are not shown for U2002 power meter

Question asked by tamerabuelfadl on Mar 12, 2015
I got some little problem when making trace plot of the power envelope using U2002A USB power sensor module. The two markers which is supposed to give reading X and Y for Marker 1A and 1B, do not show any readings with the two dashs "--". Did any body face similar problem? and is there any solution to it?

Thanks,
Tamer

Outcomes