AnsweredAssumed Answered

want to measure only S11 & S21 with 2-port full cal?

Question asked by hugorain73@gmail.com on Sep 2, 2009
Latest reply on Sep 2, 2009 by hugorain73@gmail.com
After I finish the 2-port calibration, I hit Trigger -> Single, and the analyzer Port 1 will light up for a full sweep, followed by Port 2, and the S2P file will have complete S11, S21, S12, and S22 data. However, I want to measure only S11 & S21. What can I do to skip the 2nd sweep (with Port 2 lighting up) to save time? Thank you.  

Outcomes