AnsweredAssumed Answered

PNA Check Sweep Complete VI Labview

Question asked by Zzimmha42 on Aug 27, 2015
Latest reply on Sep 2, 2015 by mr_matt
Hey, I currently am working on a project in labview utilizing a hand full of different Agilent Network Analyzer models (5230A, 5230C, 5234A, 5227A, 5232A, and 5235A). In my program I use an AGPNA VI called check sweep complete. I use this VI to trigger a single sweep, go into hold, and then read the data from that sweep. I am running into an issue with this particular VI, on occasion it does not wait for the sweep to be completed before the data is read, making for a very inaccurate plot of data. Has anyone run into issues with using the particular VI in labview? Attached are a screen shot of the check for sweep code and subsequent SCPI commands. Thanks.  

Attachments

Outcomes