AnsweredAssumed Answered

Auto export of data with Benchlink Data Logger 3

Question asked by gabe on Jul 13, 2015
Hi, I'd like to know if there is a way to have Benchlink Data Logger 3 automatically save data within a configured scan at certain points...ie every 30mins or 100 relay counts, etc.  Also then append the previous data with the new data all within one spreadsheet.  Is this possible or do I have to upgrade to Benchlink Data Logger Pro version and write a script to do this?

I'd like to run a very long scan and be sure the data is being backed up.  It's also nice to be able to view the data outside of Benchlink while the same configured scan is still running.

I'm using an Agilent 34970A with three 34901A modules.

Thanks for all your help!
Gabe  

Outcomes