AnsweredAssumed Answered

Solid=State Switch replacement in 8753D ?

Question asked by S.Reeves on Mar 14, 2016
Latest reply on Mar 22, 2017 by BoinFinland
While the part may be still available for replacement of the 8753D Solid-State switch, part # 5086-7539 is is rather pricey at $ 4531.

Can the Keysight switch model U9397A be used, although the low frequency is spec'd only down to 300 kHz. The low end of the 8753D is 30 kHz.

Steve  

Outcomes