AnsweredAssumed Answered

Mem upgrade 335MEM2U

Question asked by audioguy on Jun 7, 2015
Latest reply on Jul 3, 2015 by audioguy
Hi!

I wonder if anyone knows if the free mem upgrade 335MEM2U is only for generators bought as an ARB-generator, or if upgraded units also are included.

I'm about to purchase a two channel non ARB 33500 series generator and will upgrade it to ARB status. 

On this side: https://www.keysight.com/main/editorial.jspx?cc=AE&lc=eng&ckey=2496226&id=2496226

You can read: Do you own the Trueform waveform generator? Fill in the form to get your memory upgrade for FREE! Submit your details and get access to a library of sample signals and other technical content.

Eligible models: 33511B, 33512B, 33521B, 33522B, 33611A, 33612A, 33621A, 33622A

Basically I will buy a 33520 unit and turn it into a "33522" with the ARB upgrade.

Thanks in advance.  

Outcomes