AnsweredAssumed Answered

SCPI code for U8903A function

Question asked by pdas on Jan 21, 2016
Hello, 

I was wondering if someone knows what the SCPI command is to run on the Channel Run/Stop button remotely using SCPI commands (through LabVIEW VIs). I know the :OUTP:STAT command turns both the Output and Channel buttons on when in the Generator mode, but not in the Analyzer mode. So what command specifically turns on the Channel Run/Stop when in Analyzer mode?

Thanks.

Edited by: pdas on Jan 21, 2016 12:45 PM  

Outcomes