While attempting to load the recent firmware release "3.05 - 2015-12-21" for the 33500B series generators, the instrument responds with the new firmware being older or the same as the current version.
My current version is 3.03. Having downloaded the new USB version of 3.05 and looking at the file "build.xml" it has the following:
03.03 Agilent 33500 Series Rev A.03.03 NOTE: Front panel may go blank for about 30 seconds on first reboot. Refer to release notes. 1/14/2014 11:21:16 AM
I've also tried the 3.05 LAN version and used the Keysight Firmware Update program to create the files on a USB drive but the response from the instrument is the same error.
Thanks
Andrew
My current version is 3.03. Having downloaded the new USB version of 3.05 and looking at the file "build.xml" it has the following:
I've also tried the 3.05 LAN version and used the Keysight Firmware Update program to create the files on a USB drive but the response from the instrument is the same error.
Thanks
Andrew
Using the Keysight Firmware Update application prepared a USB stick, freshly formatted, making sure to respond "No" to the "Is the Revision string...1.14" as the current firmware is "3.03-1.19-2.00-52-00", I think that means the revision string is "1.19"?
The usb stick contains the xml file, part of which has the following:
Still the same error "The firmware version on USB drive is the same as or older than the current firmware."
User error perhaps?