Hello,
I was using ADS 2012 to simulate copper matching circuits of Power amplifier. Copper matching is created or copied from Gerber file. Ports were attached to add matching capacitors and EM simulation is done. In the schematics, this EM model is dragged in. Capacitors are added at the matching ports (Mainly Modelthics caps) and S parameter simulation is done.
In ADS 2014, I could see EM Co-Simulation in the EM setup ?. How this feature can be used in the above mentioned situation?. Can I use the Modelthics cap model in the Layout itself?
Leyo Joseph
I was using ADS 2012 to simulate copper matching circuits of Power amplifier. Copper matching is created or copied from Gerber file. Ports were attached to add matching capacitors and EM simulation is done. In the schematics, this EM model is dragged in. Capacitors are added at the matching ports (Mainly Modelthics caps) and S parameter simulation is done.
In ADS 2014, I could see EM Co-Simulation in the EM setup ?. How this feature can be used in the above mentioned situation?. Can I use the Modelthics cap model in the Layout itself?
Leyo Joseph