AnsweredAssumed Answered

Should the 7 mm broadband load in the 85050B or 85050C kits have a collet?

Question asked by drkirkby on Aug 17, 2014
Latest reply on Aug 20, 2014 by drkirkby
I've got two 7 mm kits with the broadband load 85050-60006. Neither have a collet, but just a centre conductor with a hole on it, which is different to any other APC7 connector I ever recall seeing. Is this correct, or do both have missing collets? Compare pictures above to a lowband load, which has a standard collect I have seen many times. 

It is odd these broadband loads have metal protective caps, which I have never understood. Now I am wondering if its due to the lack of a collet. 

Dave  

Outcomes